LeadAngles Class¶
-
class
NXOpen.CAM.
LeadAngles
¶ Bases:
NXOpen.TaggedObject
Represents a lead angles
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
AtLeadingEdge | Returns or sets the lead angle at leading edge |
AtTrailingEdge | Returns or sets the lead angle at trailing edge |
ControlType | Returns or sets the lead angle control type |
Tag | Returns the Tag for this object. |
Methods¶
Enumerations¶
LeadAnglesControlTypes Enumeration | Available types for lead angle control type |
Property Detail¶
AtLeadingEdge¶
-
LeadAngles.
AtLeadingEdge
¶ Returns or sets the lead angle at leading edge
-------------------------------------
Getter Method
Signature
AtLeadingEdge()
Returns: the lead angle at leading edge Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AtLeadingEdge(leadAngle)
Parameters: leadAngle (float) – the lead angle at leading edge New in version NX8.5.0.
License requirements: cam_base (“CAM BASE”)
AtTrailingEdge¶
-
LeadAngles.
AtTrailingEdge
¶ Returns or sets the lead angle at trailing edge
-------------------------------------
Getter Method
Signature
AtTrailingEdge()
Returns: the lead angle at trailing edge Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AtTrailingEdge(leadAngle)
Parameters: leadAngle (float) – the lead angle at trailing edge New in version NX8.5.0.
License requirements: cam_base (“CAM BASE”)
ControlType¶
-
LeadAngles.
ControlType
¶ Returns or sets the lead angle control type
-------------------------------------
Getter Method
Signature
ControlType()
Returns: the lead angle control type Return type: NXOpen.CAM.LeadAnglesControlTypes
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ControlType(leadAngleType)
Parameters: leadAngleType ( NXOpen.CAM.LeadAnglesControlTypes
) – the lead angle control typeNew in version NX8.5.0.
License requirements: cam_base (“CAM BASE”)