InspectionSensorMassEditBuilderSensorStrategyType Enumeration

NXOpen.CAM.InspectionSensorMassEditBuilder.SensorStrategyType is an alias for NXOpen.CAM.InspectionSensorMassEditBuilderSensorStrategyType

class NXOpen.CAM.InspectionSensorMassEditBuilderSensorStrategyType

Bases: object

the sensor strategy

Enum Members

Enum Member Enum Member Description
Createasneeded
Create as needed
Useexistingonly
Use existing only
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.