InspectionSensorMassEditBuilderSensorSelectModeType Enumeration

NXOpen.CAM.InspectionSensorMassEditBuilder.SensorSelectModeType is an alias for NXOpen.CAM.InspectionSensorMassEditBuilderSensorSelectModeType

class NXOpen.CAM.InspectionSensorMassEditBuilderSensorSelectModeType

Bases: object

the sensor selection mode

Enum Members

Enum Member Enum Member Description
Automatic
Choose sensor automatically
SpecifySensor
Manually specify sensor
SpecifyProbeAngles
Manually specify probe angles
SpecifyProbeTip
Manually specify probe tip
SpecifyAnglesandTip
Manually specify probe angles and probe tip
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.