InspectionSensorBuilderSensorTypes Enumeration

NXOpen.CAM.InspectionSensorBuilder.SensorTypes is an alias for NXOpen.CAM.InspectionSensorBuilderSensorTypes

class NXOpen.CAM.InspectionSensorBuilderSensorTypes

Bases: object

the sensor type

Enum Members

Enum Member Enum Member Description
Fixed
Fixed
Index
Indexable
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.