InspectionPathPointBuilder Class¶
-
class
NXOpen.CAM.
InspectionPathPointBuilder
¶ Bases:
NXOpen.TaggedObject
Represents an inspection path point builder
New in version NX8.5.0.
Methods¶
Method | Description |
---|---|
Delete | Delete an existing path point |
GetPointData | Get the values of an existing path point |
ModifyData | Modify an existing path point, name changed if not unique |
SetPointData | Create a new path point, name changed if not unique |
Method Detail¶
Delete¶
-
InspectionPathPointBuilder.
Delete
¶ Delete an existing path point
Signature
Delete(index)
Parameters: index (int) – the index of the path point to delete New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
GetPointData¶
-
InspectionPathPointBuilder.
GetPointData
¶ Get the values of an existing path point
Signature
GetPointData(index)
Parameters: index (int) – the index of the path point Returns: a tuple Return type: A tuple consisting of (point, angleA, angleB). point is a NXOpen.NXObject
. the selected point angleA is a float. the A angle angleB is a float. the B angleNew in version NX8.5.0.
License requirements: None.
ModifyData¶
-
InspectionPathPointBuilder.
ModifyData
¶ Modify an existing path point, name changed if not unique
Signature
ModifyData(index, point, angleA, angleB)
Parameters: - index (int) – the index of the path point to modify
- point (
NXOpen.NXObject
) – the selected point - angleA (float) – the A angle
- angleB (float) – the B angle
New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SetPointData¶
-
InspectionPathPointBuilder.
SetPointData
¶ Create a new path point, name changed if not unique
Signature
SetPointData(index, point, angleA, angleB)
Parameters: - index (int) – the index after which the new path point will be added
- point (
NXOpen.NXObject
) – the new path point - angleA (float) – the A angle
- angleB (float) – the B angle
New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)