InspectionPathBuilderEntryExitType Enumeration

NXOpen.CAM.InspectionPathBuilder.EntryExitType is an alias for NXOpen.CAM.InspectionPathBuilderEntryExitType

class NXOpen.CAM.InspectionPathBuilderEntryExitType

Bases: object

the entry/exit flag

Enum Members

Enum Member Enum Member Description
Entry
Entry Point
Exit
Exit Point
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.