InspectionOperationTransformBuilderMotion Enumeration

NXOpen.CAM.InspectionOperationTransformBuilder.Motion is an alias for NXOpen.CAM.InspectionOperationTransformBuilderMotion

class NXOpen.CAM.InspectionOperationTransformBuilderMotion

Bases: object

Motion Type

Enum Members

Enum Member Enum Member Description
Delta
motion delta
ToAPoint
motion to a point
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.