InspectionOperationTransformBuilderAngle Enumeration

NXOpen.CAM.InspectionOperationTransformBuilder.Angle is an alias for NXOpen.CAM.InspectionOperationTransformBuilderAngle

class NXOpen.CAM.InspectionOperationTransformBuilderAngle

Bases: object

Angle Type

Enum Members

Enum Member Enum Member Description
Specify
specify a angle
TwoPoint
use two point to sepcify a angle
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.