InspectionMoveBuilderTipModeTypes Enumeration

NXOpen.CAM.InspectionMoveBuilder.TipModeTypes is an alias for NXOpen.CAM.InspectionMoveBuilderTipModeTypes

class NXOpen.CAM.InspectionMoveBuilderTipModeTypes

Bases: object

the tip selection mode

Enum Members

Enum Member Enum Member Description
Auto
Auto specify
Specify
Manual specify
Existing
From existing sensor
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.