InspectionMeasurePointBuilderPointTypes Enumeration

NXOpen.CAM.InspectionMeasurePointBuilder.PointTypes is an alias for NXOpen.CAM.InspectionMeasurePointBuilderPointTypes

class NXOpen.CAM.InspectionMeasurePointBuilderPointTypes

Bases: object

specifies the method used to define a point

Enum Members

Enum Member Enum Member Description
ExistingPoint
Select an existing point
CursorLocation
Cursor Location
PointConstructor
Use the Point Constructor
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.