InspectionGraphicalReportOutputBuilder Class¶
-
class
NXOpen.CAM.
InspectionGraphicalReportOutputBuilder
¶ Bases:
NXOpen.Builder
Represents the builder for Inspection Graphical Report Output.
This class is used to publish Inspection graphical reports for the end user. To create a new instance of this class, use
NXOpen.CAM.InspectionOperationCollection.CreateGraphicalReportOutputBuilder()
New in version NX10.0.3.
Properties¶
Property | Description |
---|---|
OpenFile | Returns or sets the open file option |
OutputFile | Returns or sets the output file |
OutputFormat | Returns or sets the output format |
PageOrientation | Returns or sets the page orientation |
PageSize | Returns or sets the page size |
ScaleFactor | Returns or sets the scale factor |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
Publish | Output the graphical reports |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
InspectionGraphicalReportOutputBuilderOutputFormatType Enumeration | the output format type |
InspectionGraphicalReportOutputBuilderPageOrientationType Enumeration | the page orientation type |
InspectionGraphicalReportOutputBuilderPageSizeType Enumeration | the page size type |
Property Detail¶
OpenFile¶
-
InspectionGraphicalReportOutputBuilder.
OpenFile
¶ Returns or sets the open file option
-------------------------------------
Getter Method
Signature
OpenFile()
Returns: Return type: bool New in version NX10.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
OpenFile(openFile)
Parameters: openFile (bool) – New in version NX10.0.3.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
OutputFile¶
-
InspectionGraphicalReportOutputBuilder.
OutputFile
¶ Returns or sets the output file
-------------------------------------
Getter Method
Signature
OutputFile()
Returns: Return type: str New in version NX10.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
OutputFile(filename)
Parameters: filename (str) – New in version NX10.0.3.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
OutputFormat¶
-
InspectionGraphicalReportOutputBuilder.
OutputFormat
¶ Returns or sets the output format
-------------------------------------
Getter Method
Signature
OutputFormat()
Returns: Return type: NXOpen.CAM.InspectionGraphicalReportOutputBuilderOutputFormatType
New in version NX10.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
OutputFormat(format)
Parameters: format ( NXOpen.CAM.InspectionGraphicalReportOutputBuilderOutputFormatType
) –New in version NX10.0.3.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
PageOrientation¶
-
InspectionGraphicalReportOutputBuilder.
PageOrientation
¶ Returns or sets the page orientation
-------------------------------------
Getter Method
Signature
PageOrientation()
Returns: Return type: NXOpen.CAM.InspectionGraphicalReportOutputBuilderPageOrientationType
New in version NX10.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
PageOrientation(pageOrientation)
Parameters: pageOrientation ( NXOpen.CAM.InspectionGraphicalReportOutputBuilderPageOrientationType
) –New in version NX10.0.3.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
PageSize¶
-
InspectionGraphicalReportOutputBuilder.
PageSize
¶ Returns or sets the page size
-------------------------------------
Getter Method
Signature
PageSize()
Returns: Return type: NXOpen.CAM.InspectionGraphicalReportOutputBuilderPageSizeType
New in version NX10.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
PageSize(pageSize)
Parameters: pageSize ( NXOpen.CAM.InspectionGraphicalReportOutputBuilderPageSizeType
) –New in version NX10.0.3.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ScaleFactor¶
-
InspectionGraphicalReportOutputBuilder.
ScaleFactor
¶ Returns or sets the scale factor
-------------------------------------
Getter Method
Signature
ScaleFactor()
Returns: Return type: float New in version NX10.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
ScaleFactor(scaleFactor)
Parameters: scaleFactor (float) – New in version NX10.0.3.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Method Detail¶
Publish¶
-
InspectionGraphicalReportOutputBuilder.
Publish
¶ Output the graphical reports
Signature
Publish(currentView)
Parameters: currentView (int) – CAM_SETUP_view New in version NX10.0.3.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Validate¶
-
InspectionGraphicalReportOutputBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.