InspectionConstructedFeatureBuilderMethodEnumType Enumeration¶
NXOpen.CAM.InspectionConstructedFeatureBuilder.MethodEnumType is an alias for NXOpen.CAM.InspectionConstructedFeatureBuilderMethodEnumType
-
class
NXOpen.CAM.
InspectionConstructedFeatureBuilderMethodEnumType
¶ Bases:
object
Construction Method
Enum Members
Enum Member Enum Member Description BestFit Best Fit a feature to point reducible subfeaturesTransform Transform a copy of a feature from one PCS to another PCSIntersection Intersects features to form a point plane or circle featureMinimum Finds the maximum feature measurement point in a specified directionMaximum Finds the minimum feature measurement point in a specified directionProjection Projects a measurement point onto a measured or nominal featureMoveByFeature Moves a copy of a point reducible feature in a direction associated with another featureMoveByVector Moves a copy of a point reducible feature in a user specifiec directionPerpendicularTo Creates a feature perpendicular to a feature and through another featureParallelTo Creates a feature parallel to a feature and through another featureOffset Creates a plane or line offset by a nominal amount to each subfeatureMiddle Creates a point, plane or line at the middle of two sub featuresConeDiameter Creates a circle at diameter of a coneConeDistance Creates a circle at distance along a coneExtract Creates a feature by extract neasurements from other features-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-