InspectionConstructedFeatureBuilderExtractEdgeDistanceType Enumeration

NXOpen.CAM.InspectionConstructedFeatureBuilder.ExtractEdgeDistanceType is an alias for NXOpen.CAM.InspectionConstructedFeatureBuilderExtractEdgeDistanceType

class NXOpen.CAM.InspectionConstructedFeatureBuilderExtractEdgeDistanceType

Bases: object

Specifies whether an extract edge distance is absolute part units or a percentage

Enum Members

Enum Member Enum Member Description
Absolute
Use an absolute distance from edge
Percentage
Use a percentage distance from edge
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.