InspectionConstructedFeatureBuilderDirectionType Enumeration¶
NXOpen.CAM.InspectionConstructedFeatureBuilder.DirectionType is an alias for NXOpen.CAM.InspectionConstructedFeatureBuilderDirectionType
-
class
NXOpen.CAM.
InspectionConstructedFeatureBuilderDirectionType
¶ Bases:
object
Specifies whether a minimum or maximum point are found using a user specified direction vector or a radial direction vector
Enum Members
Enum Member Enum Member Description SpecifiedVector Use a user specified direction vectorRadial Use a radial direction vectorFeature Use a feature (nominal/actual) for the vector-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-