InspectionConstructedFeatureBuilderConstFeatType Enumeration¶
NXOpen.CAM.InspectionConstructedFeatureBuilder.ConstFeatType is an alias for NXOpen.CAM.InspectionConstructedFeatureBuilderConstFeatType
-
class
NXOpen.CAM.
InspectionConstructedFeatureBuilderConstFeatType
¶ Bases:
object
Type of feature to be constructed
Enum Members
Enum Member Enum Member Description Point Constructed Point FeatureLine Constructed Line FeaturePlane Constructed Plane FeatureArc Constructed Arc FeatureCircle Constructed Circle FeatureCylinder Constructed Cylinder FeatureCone Constructed Cone FeatureSphere Constructed Sphere FeatureCurve Constructed Curve FeatureTorus Constructed Torus FeatureSurface Constructed Surface FeatureSlotTab Constructed Slot/Tab Feature-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-