InspectionConstructedFeatureBuilderAvailableStateType Enumeration

NXOpen.CAM.InspectionConstructedFeatureBuilder.AvailableStateType is an alias for NXOpen.CAM.InspectionConstructedFeatureBuilderAvailableStateType

class NXOpen.CAM.InspectionConstructedFeatureBuilderAvailableStateType

Bases: object

State of features in available feature list

Enum Members

Enum Member Enum Member Description
Nominal
Feature is in its nominal (design) state
Actual
Feature is an actual measured feature
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.