InspectionAnalyzeBuilderDofTypes Enumeration

NXOpen.CAM.InspectionAnalyzeBuilder.DofTypes is an alias for NXOpen.CAM.InspectionAnalyzeBuilderDofTypes

class NXOpen.CAM.InspectionAnalyzeBuilderDofTypes

Bases: object

Inspection Analysis Degrees of Freedom Types

Enum Members

Enum Member Enum Member Description
On
On
Off
Off
Tolerance
Defined by Tolerance
Limits
Specify Limits
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.