InspectionAlignmentBuilderXtMethods Enumeration

NXOpen.CAM.InspectionAlignmentBuilder.XtMethods is an alias for NXOpen.CAM.InspectionAlignmentBuilderXtMethods

class NXOpen.CAM.InspectionAlignmentBuilderXtMethods

Bases: object

PCS Translation method in X direction

Enum Members

Enum Member Enum Member Description
Distance
Translate a distance
Datum
Translate by Datum
NominalFeature
Translate by Nominal Feature
MeasuredFeature
Translate by Measured Feature
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.