InspectionAlignmentBuilderSaveStates Enumeration

NXOpen.CAM.InspectionAlignmentBuilder.SaveStates is an alias for NXOpen.CAM.InspectionAlignmentBuilderSaveStates

class NXOpen.CAM.InspectionAlignmentBuilderSaveStates

Bases: object

PCS state to save, either Actual or nominal

Enum Members

Enum Member Enum Member Description
Actual
Save Actual PCS
Nominal
Save Nominal PCS
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.