InspectionAlignmentBuilderRotationMethods Enumeration

NXOpen.CAM.InspectionAlignmentBuilder.RotationMethods is an alias for NXOpen.CAM.InspectionAlignmentBuilderRotationMethods

class NXOpen.CAM.InspectionAlignmentBuilderRotationMethods

Bases: object

PCS Rotation method

Enum Members

Enum Member Enum Member Description
Angle
Rotate by absolute angle
Datum
Rotate by Datum
NominalFeature
Rotate by Nominal Feature
MeasuredFeature
Rotate by Actual Feature
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.