InspectionAlignmentBuilderRecallStates Enumeration

NXOpen.CAM.InspectionAlignmentBuilder.RecallStates is an alias for NXOpen.CAM.InspectionAlignmentBuilderRecallStates

class NXOpen.CAM.InspectionAlignmentBuilderRecallStates

Bases: object

PCS state to recall, either internal or external

Enum Members

Enum Member Enum Member Description
Internal
Recall internal PCS
External
Recall external PCS
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.