InspectionAlignmentBuilderIterDevTypes Enumeration

NXOpen.CAM.InspectionAlignmentBuilder.IterDevTypes is an alias for NXOpen.CAM.InspectionAlignmentBuilderIterDevTypes

class NXOpen.CAM.InspectionAlignmentBuilderIterDevTypes

Bases: object

Iterate deviation type

Enum Members

Enum Member Enum Member Description
Absolute
Absolute deviation
Incremental
Incremental deviation
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.