InspectionAlignmentBuilderAlignTypes Enumeration¶
NXOpen.CAM.InspectionAlignmentBuilder.AlignTypes is an alias for NXOpen.CAM.InspectionAlignmentBuilderAlignTypes
-
class
NXOpen.CAM.
InspectionAlignmentBuilderAlignTypes
¶ Bases:
object
Alignment Operation Type
Enum Members
Enum Member Enum Member Description SetPCStoMCS Set the PCS to Machine CSSetPCStoCSYS Set the PCS to a NX CsysTranslatePCSOrigin Translate the PCSRotatePCS Rotate the PCSDefinePCSfromDatums Define the PCS from datumsIterate Iterate a set of features for convergenceDefinePCSfromActualDeviations Locate PCS from FeaturesSavePCS Save current PCSRecallPCS Recall previously saved PCSRotateTable Rotate tableSetPCStoCADABS Set the PCS to Cadabs-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-