InferredDoubleLock Enumeration

NXOpen.CAM.InferredDouble.Lock is an alias for NXOpen.CAM.InferredDoubleLock

class NXOpen.CAM.InferredDoubleLock

Bases: object

the lock statue

New in version NX7.5.0.

Enum Members

Enum Member Enum Member Description
UserDefined
Lock: User Defined
FromGeometry
Lock: From Geometry
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.