HoleMakingBuilderModelDepthTypes Enumeration

NXOpen.CAM.HoleMakingBuilder.ModelDepthTypes is an alias for NXOpen.CAM.HoleMakingBuilderModelDepthTypes

class NXOpen.CAM.HoleMakingBuilderModelDepthTypes

Bases: object

Available types for model depth in Hole Making Operation

Enum Members

Enum Member Enum Member Description
Always
always
Rule
rule
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.