HoleDrillingCutParameters Class¶
-
class
NXOpen.CAM.
HoleDrillingCutParameters
¶ Bases:
NXOpen.CAM.HoleMachiningCutParameters
Represents a HoleDrillingCutParameters Builder
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
BottomOffset | Returns the bottom offset |
BottomStock | Returns the bottom stock |
CheckIpwCollisions | Returns or sets the value to Check for Ipw Collsions |
CheckSafeClearance | Returns the Check Safe Clearance |
HolderClearance | Returns the Holder Clearance |
IpwType | Returns or sets the IPW type |
NeckClearance | Returns the Neck Clearance |
PartSafeClearance | Returns the Part Safe Clearance |
PartStock | Returns the part stock |
RaptoOffset | Returns the rapto offset |
ShankClearance | Returns the Shank Clearance |
Tag | Returns the Tag for this object. |
Tolerances | Returns the Tolerances builder |
TopOffset | Returns the top offset |
UseToolHolder | Returns or sets the use tool holder |
Methods¶
Property Detail¶
BottomOffset¶
-
HoleDrillingCutParameters.
BottomOffset
¶ Returns the bottom offset
-------------------------------------
Getter Method
Signature
BottomOffset()
Returns: the bottom offset Return type: NXOpen.CAM.VerticalPosition
New in version NX9.0.0.
License requirements: None.
RaptoOffset¶
-
HoleDrillingCutParameters.
RaptoOffset
¶ Returns the rapto offset
-------------------------------------
Getter Method
Signature
RaptoOffset()
Returns: the rapto offset Return type: NXOpen.CAM.VerticalPosition
New in version NX9.0.0.
License requirements: None.