HoleBossGeomHoleBossTypes Enumeration¶
NXOpen.CAM.HoleBossGeom.HoleBossTypes is an alias for NXOpen.CAM.HoleBossGeomHoleBossTypes
-
class
NXOpen.CAM.
HoleBossGeomHoleBossTypes
¶ Bases:
object
the hole or boss types
New in version NX7.5.0.
Enum Members
Enum Member Enum Member Description Hole Type: HoleBoss Type: BossThreadedHole Type: Threaded HoleThreadedBoss Type: Threaded BossCenterHole Type: Center HoleChamferHole Type: Chamfer Hole-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-