HoleBossGeomDepthLimitTypes Enumeration¶
NXOpen.CAM.HoleBossGeom.DepthLimitTypes is an alias for NXOpen.CAM.HoleBossGeomDepthLimitTypes
-
class
NXOpen.CAM.
HoleBossGeomDepthLimitTypes
¶ Bases:
object
the depth limit types
New in version NX7.5.0.
Deprecated since version NX8.0.0: The property that used this enum is replaced by
NXOpen.CAM.HoleBossSet.DepthLimit()
.Enum Members
Enum Member Enum Member Description Through Depth Limit: ThroughBlind Depth Limit: BlindUnknown It maybe mixed type with both Through and Blind features in NX8. Please use HoleBossSet builder to get the type-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-