GroupFeatures Class¶
-
class
NXOpen.CAM.
GroupFeatures
¶ Bases:
NXOpen.Builder
Represents the group features command
To create a new instance of this class, use
NXOpen.CAM.NCGroupCollection.CreateGroupFeatures()
Default values.
Property Value FeaturesToGroupType All GroupByAttributes Predefined GroupByMachiningAccessDirection false New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
FeaturesToGroupType | Returns or sets the features to group enumeration |
GeometryLocation | Returns or sets the geometry location |
GroupByAttributes | Returns or sets the group by attributes options - None, All, Predefined |
GroupByIdenticalAttributes | Returns or sets the group by identical attributes flag |
GroupByMachiningAccessDirection | Returns or sets the group by machining access direction flag |
Tag | Returns the Tag for this object. |
TopFaceCollector | Returns the top face collector |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CreateFeatureGroups | Create the feature groups |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetFeatureTypes | Set the feature types to filter |
SetInputFeatures | Set the list of input features |
SetMachiningAccessDirections | Set the machining access directions to filter |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
GroupFeaturesFeaturesToGroupTypes Enumeration | Available types for the features to group |
Property Detail¶
FeaturesToGroupType¶
-
GroupFeatures.
FeaturesToGroupType
¶ Returns or sets the features to group enumeration
-------------------------------------
Getter Method
Signature
FeaturesToGroupType()
Returns: Return type: NXOpen.CAM.GroupFeaturesFeaturesToGroupTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FeaturesToGroupType(groupType)
Parameters: groupType ( NXOpen.CAM.GroupFeaturesFeaturesToGroupTypes
) –New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
GeometryLocation¶
-
GroupFeatures.
GeometryLocation
¶ Returns or sets the geometry location
-------------------------------------
Getter Method
Signature
GeometryLocation()
Returns: Return type: str New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GeometryLocation(geometryLocation)
Parameters: geometryLocation (str) – New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
GroupByAttributes¶
-
GroupFeatures.
GroupByAttributes
¶ Returns or sets the group by attributes options - None, All, Predefined
-------------------------------------
Getter Method
Signature
GroupByAttributes()
Returns: Return type: str New in version NX9.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
GroupByAttributes(groupBy)
Parameters: groupBy (str) – New in version NX9.0.1.
License requirements: cam_base (“CAM BASE”)
GroupByIdenticalAttributes¶
-
GroupFeatures.
GroupByIdenticalAttributes
¶ Returns or sets the group by identical attributes flag
-------------------------------------
Getter Method
Signature
GroupByIdenticalAttributes()
Returns: Return type: bool New in version NX9.0.0.
Deprecated since version NX9.0.1: Use
CAM.GroupFeatures.GroupByAttributes`()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
GroupByIdenticalAttributes(enable)
Parameters: enable (bool) – New in version NX9.0.0.
Deprecated since version NX9.0.1: Use
CAM.GroupFeatures.GroupByAttributes`()
instead.License requirements: cam_base (“CAM BASE”)
GroupByMachiningAccessDirection¶
-
GroupFeatures.
GroupByMachiningAccessDirection
¶ Returns or sets the group by machining access direction flag
-------------------------------------
Getter Method
Signature
GroupByMachiningAccessDirection()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GroupByMachiningAccessDirection(enable)
Parameters: enable (bool) – New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
TopFaceCollector¶
-
GroupFeatures.
TopFaceCollector
¶ Returns the top face collector
-------------------------------------
Getter Method
Signature
TopFaceCollector()
Returns: Return type: NXOpen.ScCollector
New in version NX9.0.0.
License requirements: None.
Method Detail¶
CreateFeatureGroups¶
-
GroupFeatures.
CreateFeatureGroups
¶ Create the feature groups
Signature
CreateFeatureGroups()
New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
SetFeatureTypes¶
-
GroupFeatures.
SetFeatureTypes
¶ Set the feature types to filter
Signature
SetFeatureTypes(ftrTypes)
Parameters: ftrTypes (list of str) – New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
SetInputFeatures¶
-
GroupFeatures.
SetInputFeatures
¶ Set the list of input features
Signature
SetInputFeatures(ftrs)
Parameters: ftrs (list of NXOpen.CAM.CAMFeature
) –New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
SetMachiningAccessDirections¶
-
GroupFeatures.
SetMachiningAccessDirections
¶ Set the machining access directions to filter
Signature
SetMachiningAccessDirections(vecDirectionTags, dTolerance)
Parameters: - vecDirectionTags (list of
NXOpen.Direction
) – - dTolerance (float) –
New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
- vecDirectionTags (list of
Validate¶
-
GroupFeatures.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.