GrooveToolBuilderInsertShapes Enumeration¶
NXOpen.CAM.GrooveToolBuilder.InsertShapes is an alias for NXOpen.CAM.GrooveToolBuilderInsertShapes
-
class
NXOpen.CAM.
GrooveToolBuilderInsertShapes
¶ Bases:
object
The available insert shapes for groove tools
Enum Members
Enum Member Enum Member Description Std Standard groove toolFnr Full nose radius groove toolRtj Ring type joint groove toolUser user defined groove tool-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-