GrooveToolBuilderHolderStyles Enumeration¶
NXOpen.CAM.GrooveToolBuilder.HolderStyles is an alias for NXOpen.CAM.GrooveToolBuilderHolderStyles
-
class
NXOpen.CAM.
GrooveToolBuilderHolderStyles
¶ Bases:
object
The available holder style options for groove tools
Enum Members
Enum Member Enum Member Description Deg0 0 degreesDeg45 45 degreesDeg90 90 degreesUserDefined user defined-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-