GrooveToolBuilderHolderHands Enumeration¶
NXOpen.CAM.GrooveToolBuilder.HolderHands is an alias for NXOpen.CAM.GrooveToolBuilderHolderHands
-
class
NXOpen.CAM.
GrooveToolBuilderHolderHands
¶ Bases:
object
The available holder hand options for groove tools
Enum Members
Enum Member Enum Member Description Left0 Left hand, 0 degreesLeft90 Left hand, 90 degreesRight0 Right hand, 0 degreesRight90 Right hand, 90 degrees-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-