GrooveToolBuilderHolderGrooveHands Enumeration

NXOpen.CAM.GrooveToolBuilder.HolderGrooveHands is an alias for NXOpen.CAM.GrooveToolBuilderHolderGrooveHands

class NXOpen.CAM.GrooveToolBuilderHolderGrooveHands

Bases: object

The available holder groove hand options for groove tools

Enum Members

Enum Member Enum Member Description
Left
Left hand
Right
Right hand
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.