GrooveMillingBuilderLevelSequencingType Enumeration

NXOpen.CAM.GrooveMillingBuilder.LevelSequencingType is an alias for NXOpen.CAM.GrooveMillingBuilderLevelSequencingType

class NXOpen.CAM.GrooveMillingBuilderLevelSequencingType

Bases: object

Available types for level sequencing

Enum Members

Enum Member Enum Member Description
CeilingToFloor
Ceiling to Floor
FloorToCeiling
Floor to Ceiling
CenterCeilingFloor
Start in Center then Ceiling then Floor
CenterFloorCeiling
Start in Center then Floor then Ceiling
CenterAlternateCeilingFirst
Center Alternate, Ceiling First
CenterAlternateFloorFirst
Center Alternate, Floor First
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.