GeometryGroupOrientationTypes Enumeration

NXOpen.CAM.GeometryGroup.OrientationTypes is an alias for NXOpen.CAM.GeometryGroupOrientationTypes

class NXOpen.CAM.GeometryGroupOrientationTypes

Bases: object

the derived blank orientation types

Enum Members

Enum Member Enum Member Description
Mcs
derived blank orientation using MCS
Specify
derived blank orientation using user defined
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.