GeometryGroupDirectionTypes Enumeration

NXOpen.CAM.GeometryGroup.DirectionTypes is an alias for NXOpen.CAM.GeometryGroupDirectionTypes

class NXOpen.CAM.GeometryGroupDirectionTypes

Bases: object

the derived blank direction types

Enum Members

Enum Member Enum Member Description
Zm
derived blank direction using ZM
Specify
derived blank direction using user defined
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.