GeometryGroupBlankDefinitionTypes Enumeration¶
NXOpen.CAM.GeometryGroup.BlankDefinitionTypes is an alias for NXOpen.CAM.GeometryGroupBlankDefinitionTypes
-
class
NXOpen.CAM.
GeometryGroupBlankDefinitionTypes
¶ Bases:
object
the blank definition types
Enum Members
Enum Member Enum Member Description FromGeometry blank defined through selected geometryOffsetFromPart blank defined through offset from partAutoBlock blank defined through auto block around partIpw blank defined through IPWBoundingCylinder blank defined through bounding cylinderPartOutline blank defined through part outlinePartConvexHull blank defined through part convex hull-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-