FollowGeometryMoveBuilder Class

class NXOpen.CAM.FollowGeometryMoveBuilder

Bases: NXOpen.CAM.MoveBuilder

Represents the Follow Geometry Move Builder

This is an abstract class, and cannot be created.

New in version NX8.0.0.

Properties

Property Description
EndExtension Returns or sets the end extension
FeedRate Returns or sets the feed rate
FeedType Returns or sets the feed type
FeedUnit Returns or sets the feed unit
MotionType Returns or sets the motion type
NumberOfUserParameters Returns the number of user parameters
ProtectedMove Returns or sets the protected move status
StartExtension Returns or sets the start extension
StartPoint Returns or sets the start location
StartToolAxis Returns or sets the start tool axis
SubopLabel Returns or sets the subop label
Tag Returns the Tag for this object.

Methods

Method Description
Commit Commits any edits that have been applied to the builder.
Destroy Deletes the builder, and cleans up any objects created by the builder.
GetCommittedObjects For builders that create more than one object, this method returns the objects that are created by commit.
GetObject Returns the object currently being edited by this builder.
GetUserParameter Returns the custom parameter with the given name.
SetParent Set parent
SetSibling Set sibling
ShowResults Updates the model to reflect the result of an edit to the model for all builders that support showing results.
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

EndExtension

FollowGeometryMoveBuilder.EndExtension

Returns or sets the end extension

-------------------------------------

Getter Method

Signature EndExtension()

Returns:
Return type:NXOpen.CAM.InheritableToolDepBuilder

New in version NX8.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature EndExtension(builderTag)

Parameters:builderTag (NXOpen.CAM.InheritableToolDepBuilder) –

New in version NX8.0.0.

License requirements: cam_base (“CAM BASE”)

StartExtension

FollowGeometryMoveBuilder.StartExtension

Returns or sets the start extension

-------------------------------------

Getter Method

Signature StartExtension()

Returns:
Return type:NXOpen.CAM.InheritableToolDepBuilder

New in version NX8.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature StartExtension(builderTag)

Parameters:builderTag (NXOpen.CAM.InheritableToolDepBuilder) –

New in version NX8.0.0.

License requirements: cam_base (“CAM BASE”)

StartPoint

FollowGeometryMoveBuilder.StartPoint

Returns or sets the start location

-------------------------------------

Getter Method

Signature StartPoint()

Returns:
Return type:NXOpen.Point

New in version NX8.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature StartPoint(location)

Parameters:location (NXOpen.Point) –

New in version NX8.0.0.

License requirements: cam_base (“CAM BASE”)

StartToolAxis

FollowGeometryMoveBuilder.StartToolAxis

Returns or sets the start tool axis

-------------------------------------

Getter Method

Signature StartToolAxis()

Returns:
Return type:NXOpen.Direction

New in version NX8.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature StartToolAxis(vec)

Parameters:vec (NXOpen.Direction) –

New in version NX8.0.0.

License requirements: cam_base (“CAM BASE”)

Method Detail

Validate

FollowGeometryMoveBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.