FirstPlunge Class¶
-
class
NXOpen.CAM.
FirstPlunge
¶ Bases:
NXOpen.TaggedObject
Represents the first plunge
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
AxialCoordinate | Returns the axial coordinate |
Point | Returns or sets the first plunge point |
Position | Returns or sets the first plunge position |
RadialCoordinate | Returns the radial coordinate |
Tag | Returns the Tag for this object. |
Methods¶
Enumerations¶
FirstPlungePositions Enumeration | the first plunge positions |
Property Detail¶
AxialCoordinate¶
-
FirstPlunge.
AxialCoordinate
¶ Returns the axial coordinate
-------------------------------------
Getter Method
Signature
AxialCoordinate()
Returns: the axial builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
Point¶
-
FirstPlunge.
Point
¶ Returns or sets the first plunge point
-------------------------------------
Getter Method
Signature
Point()
Returns: the first plunge point Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Point(point)
Parameters: point ( NXOpen.Point
) – the first plunge pointNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
Position¶
-
FirstPlunge.
Position
¶ Returns or sets the first plunge position
-------------------------------------
Getter Method
Signature
Position()
Returns: the first plunge position Return type: NXOpen.CAM.FirstPlungePositions
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Position(position)
Parameters: position ( NXOpen.CAM.FirstPlungePositions
) – the first plunge positionNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
RadialCoordinate¶
-
FirstPlunge.
RadialCoordinate
¶ Returns the radial coordinate
-------------------------------------
Getter Method
Signature
RadialCoordinate()
Returns: the radial builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.