FeedsOptimizationDataFeedRateRangeType Enumeration

NXOpen.CAM.FeedsOptimizationData.FeedRateRangeType is an alias for NXOpen.CAM.FeedsOptimizationDataFeedRateRangeType

class NXOpen.CAM.FeedsOptimizationDataFeedRateRangeType

Bases: object

The Feed Rate Range options

Enum Members

Enum Member Enum Member Description
Percent
Percent
Constant
Constant
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.