FeedsBuilderRecalcuateBasedOn Enumeration

NXOpen.CAM.FeedsBuilder.RecalcuateBasedOn is an alias for NXOpen.CAM.FeedsBuilderRecalcuateBasedOn

class NXOpen.CAM.FeedsBuilderRecalcuateBasedOn

Bases: object

The recalculation based on attribute

New in version NX8.0.0.

Enum Members

Enum Member Enum Member Description
SurfaceSpeed
surface speed
SpindleSpeed
spindle speed
FeedPerTooth
feed per tooth
CutFeedRate
cut feed rate
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.