FeatureRecognitionBuilderGeometrySearch Enumeration¶
NXOpen.CAM.FeatureRecognitionBuilder.GeometrySearch is an alias for NXOpen.CAM.FeatureRecognitionBuilderGeometrySearch
-
class
NXOpen.CAM.
FeatureRecognitionBuilderGeometrySearch
¶ Bases:
object
the geometry search type
Enum Members
Enum Member Enum Member Description Workpiece Search for features in workpieceAllGeometry Search for features in all geometrySelected Search for features in user-selected geometry-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-