FeatureProcessBuilderFeatureGroupingType Enumeration¶
NXOpen.CAM.FeatureProcessBuilder.FeatureGroupingType is an alias for NXOpen.CAM.FeatureProcessBuilderFeatureGroupingType
-
class
NXOpen.CAM.
FeatureProcessBuilderFeatureGroupingType
¶ Bases:
object
Determines how features are allocated to feature groups
Enum Members
Enum Member Enum Member Description AlwaysCreateNew Always create a new feature groupPerFeature Create a feature group per featureUseExisting Try to use existing feature groups-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-