FeatureSet Class¶
-
class
NXOpen.CAM.FBM.
FeatureSet
¶ Bases:
NXOpen.CAM.GeometrySet
Interface for feature set
To create a new instance of this class, use
NXOpen.CAM.FBM.FeatureGeometry.CreateFeatureSet()
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
AngleToleranceEdges | Returns or sets the angle tolerance |
BoundaryEdges | Returns the boundary edges selection collector for a region set |
CheckStock | Returns or sets the check stock |
CustomFeed | Returns or sets the flag whether this set has custom feed rate activated |
CustomPartOffset | Returns or sets the flag whether this set has custom part offset activated |
CustomStock | Returns or sets the flag whether this set has custom stock activated |
CustomTolerance | Returns or sets the flag whether this set has custom tolerances activated |
DraftAngle | Returns or sets the draft angle |
DriveStock | Returns or sets the drive stock |
FeedUnit | Returns or sets the feed rate unit |
FeedValue | Returns or sets the feed rate value |
FinalStock | Returns or sets the final stock |
HoleList | Returns the ignore holes builder |
IgnoreLoopsStatus | Returns or sets the ignore loops status |
InitialStock | Returns or sets the initial stock |
Intol | Returns or sets the inner tolerance value |
MaterialSide | Returns or sets the material side |
Outtol | Returns or sets the outer tolerance value |
PartOffset | Returns or sets the part offset value |
SafeClearance | Returns or sets the safe clearance |
ScCollector | Returns the sc collector |
SeedFace | Returns or sets the seed face |
Selection | Returns the selection containing the geometric entities |
Tag | Returns the Tag for this object. |
TraverseInteriorEdges | Returns or sets the traverse interior edges flag |
UseTangentEdgeAngles | Returns or sets the use tangent edge angle flag |
Methods¶
Method | Description |
---|---|
ApplyEdgeSelection | Apply Edge Selections |
CreateFeature | Creates the feature using the specified tags @return |
GetFeature | Returns the feature @return |
GetItems | Get geometry items @return |
RemoveSelectionIntent | Break selection intent, and replace all the rules with single rules. |
SetName | Set name |
Method Detail¶
CreateFeature¶
-
FeatureSet.
CreateFeature
¶ Creates the feature using the specified tags
Signature
CreateFeature(entities)
Parameters: entities (list of NXOpen.NXObject
) – the input entitiesReturns: Return type: NXOpen.CAM.FBM.Feature
New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
GetFeature¶
-
FeatureSet.
GetFeature
¶ Returns the feature
Signature
GetFeature()
Returns: Return type: NXOpen.CAM.FBM.Feature
New in version NX9.0.0.
License requirements: None.