DriveMode Class

class NXOpen.CAM.DriveMode

Bases: NXOpen.TaggedObject

Drive Mode Builder

New in version NX7.5.0.

Properties

Property Description
FloorOverlap Returns the Floor Overlap Distance
Mode Returns or sets the Drive Mode Type
ReferenceToolDiameter Returns or sets the Reference Tool Diameter
Tag Returns the Tag for this object.
WallOverlap Returns the Wall Overlap Distance

Methods

Enumerations

DriveModeType Enumeration Available types for Drive Mode

Property Detail

FloorOverlap

DriveMode.FloorOverlap

Returns the Floor Overlap Distance

-------------------------------------

Getter Method

Signature FloorOverlap()

Returns:the Floor Overlap Distance
Return type:NXOpen.CAM.InheritableDoubleBuilder

New in version NX7.5.0.

License requirements: None.

Mode

DriveMode.Mode

Returns or sets the Drive Mode Type

-------------------------------------

Getter Method

Signature Mode()

Returns:the Drive Mode
Return type:NXOpen.CAM.DriveModeType

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Mode(type)

Parameters:type (NXOpen.CAM.DriveModeType) – the Drive Mode

New in version NX7.5.0.

License requirements: None.

ReferenceToolDiameter

DriveMode.ReferenceToolDiameter

Returns or sets the Reference Tool Diameter

-------------------------------------

Getter Method

Signature ReferenceToolDiameter()

Returns:the Reference Tool Diameter
Return type:float

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ReferenceToolDiameter(toolDia)

Parameters:toolDia (float) – the Reference Tool Diameter

New in version NX7.5.0.

License requirements: None.

WallOverlap

DriveMode.WallOverlap

Returns the Wall Overlap Distance

-------------------------------------

Getter Method

Signature WallOverlap()

Returns:the Wall Overlap Distance
Return type:NXOpen.CAM.InheritableDoubleBuilder

New in version NX7.5.0.

License requirements: None.