DrillTapToolBuilderToolThreadFormMethodTypes Enumeration

NXOpen.CAM.DrillTapToolBuilder.ToolThreadFormMethodTypes is an alias for NXOpen.CAM.DrillTapToolBuilderToolThreadFormMethodTypes

class NXOpen.CAM.DrillTapToolBuilderToolThreadFormMethodTypes

Bases: object

thread form method

Enum Members

Enum Member Enum Member Description
Cutting
cutting
Roll
roll
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.