DmUserExitCiBuilder Class¶
-
class
NXOpen.CAM.
DmUserExitCiBuilder
¶ Bases:
NXOpen.TaggedObject
Represents a exit name ci Builder
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
DmUserExitCi | Returns or sets the Project Type |
Tag | Returns the Tag for this object. |
Methods¶
Property Detail¶
DmUserExitCi¶
-
DmUserExitCiBuilder.
DmUserExitCi
¶ Returns or sets the Project Type
-------------------------------------
Getter Method
Signature
DmUserExitCi()
Returns: the project type value Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DmUserExitCi(dmUserExitCiValue)
Parameters: dmUserExitCiValue (str) – the project type value New in version NX5.0.0.
License requirements: None.