DmTrimExtend Class¶
-
class
NXOpen.CAM.
DmTrimExtend
¶ Bases:
NXOpen.TaggedObject
Represents a streamline trim and extend builder
This is an abstract class and cannot be instantiated.
New in version NX10.0.1.
Properties¶
Property | Description |
---|---|
EndCut | Returns or sets the end cut |
EndStep | Returns or sets the end step |
StartCut | Returns or sets the start cut |
StartStep | Returns or sets the start step |
Tag | Returns the Tag for this object. |
Methods¶
Property Detail¶
EndCut¶
-
DmTrimExtend.
EndCut
¶ Returns or sets the end cut
-------------------------------------
Getter Method
Signature
EndCut()
Returns: the end cut Return type: float New in version NX10.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndCut(endCut)
Parameters: endCut (float) – the end cut New in version NX10.0.1.
License requirements: cam_base (“CAM BASE”)
EndStep¶
-
DmTrimExtend.
EndStep
¶ Returns or sets the end step
-------------------------------------
Getter Method
Signature
EndStep()
Returns: the end step Return type: float New in version NX10.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndStep(endStep)
Parameters: endStep (float) – the end step New in version NX10.0.1.
License requirements: cam_base (“CAM BASE”)
StartCut¶
-
DmTrimExtend.
StartCut
¶ Returns or sets the start cut
-------------------------------------
Getter Method
Signature
StartCut()
Returns: the start cut Return type: float New in version NX10.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartCut(startCut)
Parameters: startCut (float) – the start cut New in version NX10.0.1.
License requirements: cam_base (“CAM BASE”)
StartStep¶
-
DmTrimExtend.
StartStep
¶ Returns or sets the start step
-------------------------------------
Getter Method
Signature
StartStep()
Returns: the start step Return type: float New in version NX10.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartStep(startStep)
Parameters: startStep (float) – the start step New in version NX10.0.1.
License requirements: cam_base (“CAM BASE”)