DmStreamlineCutStep Class¶
-
class
NXOpen.CAM.
DmStreamlineCutStep
¶ Bases:
NXOpen.TaggedObject
Represents a streamline cut step builder
This object is a sub-object and cannot be instantiated.
New in version NX10.0.1.
Properties¶
Property | Description |
---|---|
CutStepType | Returns or sets the cut step type which defines different cut steps including tolerances and points number |
FirstCut | Returns or sets the first cut which defines point number for the first cut |
SecondCut | Returns or sets the second cut which defines point number for the second cut |
StepIntol | Returns the step Intol which defines the inner tolerance |
StepOutol | Returns the step Outol which defines the outer tolerance |
Tag | Returns the Tag for this object. |
ThirdCut | Returns or sets the third cut which defines point number for the third cut and is available when cut pattern is follow |
Methods¶
Property Detail¶
CutStepType¶
-
DmStreamlineCutStep.
CutStepType
¶ Returns or sets the cut step type which defines different cut steps including tolerances and points number
-------------------------------------
Getter Method
Signature
CutStepType()
Returns: the cut step type value Return type: NXOpen.CAM.DPMItpBuilderStepMethodOption
New in version NX10.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
CutStepType(type)
Parameters: type ( NXOpen.CAM.DPMItpBuilderStepMethodOption
) – the cut step type valueNew in version NX10.0.1.
License requirements: cam_base (“CAM BASE”)
FirstCut¶
-
DmStreamlineCutStep.
FirstCut
¶ Returns or sets the first cut which defines point number for the first cut
-------------------------------------
Getter Method
Signature
FirstCut()
Returns: the first cut value Return type: int New in version NX10.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstCut(firstCut)
Parameters: firstCut (int) – the first cut value New in version NX10.0.1.
License requirements: cam_base (“CAM BASE”)
SecondCut¶
-
DmStreamlineCutStep.
SecondCut
¶ Returns or sets the second cut which defines point number for the second cut
-------------------------------------
Getter Method
Signature
SecondCut()
Returns: the second cut value Return type: int New in version NX10.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondCut(secondCut)
Parameters: secondCut (int) – the second cut value New in version NX10.0.1.
License requirements: cam_base (“CAM BASE”)
StepIntol¶
-
DmStreamlineCutStep.
StepIntol
¶ Returns the step Intol which defines the inner tolerance
-------------------------------------
Getter Method
Signature
StepIntol()
Returns: The Step Intol Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX10.0.1.
License requirements: None.
StepOutol¶
-
DmStreamlineCutStep.
StepOutol
¶ Returns the step Outol which defines the outer tolerance
-------------------------------------
Getter Method
Signature
StepOutol()
Returns: The Step Intol Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX10.0.1.
License requirements: None.
ThirdCut¶
-
DmStreamlineCutStep.
ThirdCut
¶ Returns or sets the third cut which defines point number for the third cut and is available when cut pattern is follow
-------------------------------------
Getter Method
Signature
ThirdCut()
Returns: the third cut value Return type: int New in version NX10.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
ThirdCut(thirdCut)
Parameters: thirdCut (int) – the third cut value New in version NX10.0.1.
License requirements: cam_base (“CAM BASE”)