DmRadBuilderRadStepoverTypeType Enumeration

NXOpen.CAM.DmRadBuilder.RadStepoverTypeType is an alias for NXOpen.CAM.DmRadBuilderRadStepoverTypeType

class NXOpen.CAM.DmRadBuilderRadStepoverTypeType

Bases: object

Available types for Stepover for the Radial Cut in scop.

The enum type is obsolete.

Enum Members

Enum Member Enum Member Description
Constant Constant
Scallop Scallop
Tool Tool Diameter
Maximum Maximum
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.